Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to configure the STBEHC3020 for one shot mode

Issue
How to configure the STBEHC3020 for one shot.

Product Line
All versions of the Advantys Configuration Software.

Environment
Windows 7

Resolution
Wire the 'STBEHC3020' to the incremental encoder.
fgh

ghjy

  • Double click on the 'STBEHC3020' module to open the properties window for the module.
fghj
  • Configure the parameters as shown.
· Download the application to the island.
fghyu
  • Start the PLC.
· Place the PLC into test mode.
dfghy
  • Set the Input Validation bits to Off.
dfty
  • Enable the Counter Synch
sdf
  • Enable the Counter Enable
dfg

To reset the counter, toggle the counter sync bit from 0 to 1.