Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What could cause my Quantum 140CPU67160 to come up as 'NO CONFIG' after a power cycle?

One possible cause is that the PLC is using a PCMCIA card in slot 1 that has a bad battery. A bad battery is indicated by PCM1 with the number flashing on the LCD display. In PLC logic, %S67 (PCMCIABAT0) can be monitored.