How far away from the Circuit Monitor Series 2000 can I mount the RTM (ride-through module)?
Issue:
Customer would like to mount the RTM physically and needs to know the maximum distance allowed from the CM2000 Series.
Product Line:
CM2150
CM2250
CM2350
CM2450
Environment:
Installation of a Ride-Through Module on a CM2000 Series Meter
Cause:
Resolution:
The RTM can be mounted on the back of the Circuit Monitor or can be mounted remotely, as long as it is mounted within 10 feet of the Circuit Monitor.
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.