Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum number of Digital Inputs available on a CM4000 series meter?

Product Line
CM4000
CM4250
CM4000T

Resolution
The maximum number of Digital Inputs available on a CM4000 is 16.

Eight digital inputs are available on the I/O Extender via the IOX08 option and digital inputs are available with the digital I/O option card IOC44.

Schneider Electric Egypt and North East Africa