{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible for the CM4XXX series to detect flicker severity?
Issue
Can the CM4XXX series detect flicker severity

Product Line
CM4000
CM4250
CM4000T

Environment
Power Quality Detection

Cause
Not all CM4000 meters can detect flicker severity

Resolution
The CM4000 and CM4250, by default, do not have the capability to detect flicker severity.

To detect flickers on these meters the Current/Voltage Module Transient (CVMT) must be installed

The CM4000T by default can detect flicker severity

Schneider Electric Egypt and North East Africa