Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How to create customized screens for the CM4000 display
Issue
What is the best method for creating customized screens for the CM4000 display

Product Line
CM4000

Environment
Meter Display Configuration

Resolution
Custom displays can be programmed using the meter's remote display. There is no remote software support for local display screen development.

For instructions on how to set up these customized screens please see the CM4000 reference manual which is attached below. The instructions for setting up custom screens begin on page 35.

Here is a video which shows how to setup custom screens and view them via front display:

Schneider Electric Egypt and North East Africa

Attachment(s)
CM4000_Reference_Manual.pdf [3.41 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center