Issue
Part number for PM800 series remote display kit
Product Line
PM800 series
Environment
Part Numbers
Resolution
The part number for the PM800 series meter remote display kit is PM8RD. This part number includes the remote display, the cable (CAB12) and the 4-wire, RS232/485 communication module.
Please note there is no commercial part number for just the remote display itself. The part number for the PM800 series meter remote display adapter is PM8RDA.
The PM800 series has passed the end of commercialization period and therefore distributors may or may not carry the parts.
Released for: Schneider Electric Egypt and North East Africa