{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the part number for a CT shorting terminal block?

Issue
What is the part number for a CT shorting terminal block?


Product Line
Power Meter Accessories


Environment
All meter applications with current over 5 Amps which require Current Transformers.


Cause
Information needed on shorting terminal blocks


Resolution

For a 4-pole shorting block it is 3090TB4 and for the 6-pole it is 3090TB6

UPDATE Year 2014
Going forward any 3090TB4 or 3090TB6 Shorting Terminal Block ordered will be Cooper Bussmann branded and not Marathon branded.
3090TB6 = Cooper Bussman model KUXSC6S2644
3090TB4 = Cooper Bussman model KUXSC4S2644
*Cutsheet attached below*

The shorting screws for the 3090TB4 and 3090TB6 CT shorting blocks can be purchased from "Marathon Special PRODUCTS"
The part number for the shorting screws is "9616901". Both the 4-pole and 6-pole CT shorting blocks require a quantity of 4 of the provided screws part number.


Internal PMO/PMC
All content © 1992-2007 Schneider Electric
text
texttext
texttext

Legacy KB System (APS) Data: RESL185215 V2.0

Schneider Electric Egypt and North East Africa

Attachment(s)

3090 CT SHORTING BLOCKS 2014.pdf3090 CT SHORTING BLOCKS 2014.pdf [102.67 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.