{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I find the serial number of a CM2000 by reading registers?

Issue
Finding the serial number of a CM2000

Product Line
CM2000

Environment
Serial Number

Resolution
The CM2000 serial number can be found by reading register 2096 and 2097. Use the following formula to find the serial number. If register 2096 is negative then the Serial Number = (reg.2097 x 2^16)+(reg.2096 + 2^16). If register 2096 is positive Serial Number = (reg.2097 x 2^16)+(reg.2096)

Schneider Electric Egypt and North East Africa