How can we help you today?

How does the ION 6200 calculate I4?

Issue

One is getting I4 readings without anything wired to it.  How is this calculated?

Product Line

ION6200

Resolution

I4 is calculated from the fundamental harmonic data.
Sequence for calculation:

  • FFT on I1, I2, I3
  • add up I1,I2,I3 real and imaginary fundamental values after calibrating to give complex sum
  • get RMS from complex sum
  • transfer into I4 register.

This means for high harmonic currents, 6200 I4 will only give the I4 fundamental current and will disagree with actual current that contains all harmonics. It used to be calculated on a sample by sample basis, but since calibration of samples is impossible, it used a "merged" calibration constant at the end of RMS sums. This only worked if the calibration constants were reasonably close and caused accuracy problems, hence it was switched to the FFT method.

NOTE: the 6200 only measures up to the 15th harmonic.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center