Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
How Do I Configure Microsoft Excel To Allow Macros To Run when running reports using Repgen?

Issue
The ION Enterprise 5/6 or PME 7/8 reporter application fails to generate a report with the following error: "Your Excel security settings do not allow this waveform processing to run."




Product Line
StruxureWare Power Monitoring Expert, Reporter

Environment
ION Enterprise 5/6, Power Monitoring Expert 7/8, Microsoft Excel 2007/2010/2013/2016

Cause
The Microsoft Excel security settings are not setup to allow trust access to the VBA project object model.

Resolution

A number of the default Reporter Excel-based reports require Trust Access to the VBA project model. Follow the steps below to change this setting within Microsoft Excel 2016. Other Microsoft Excel versions will have a similar procedure.

1. Run Micrsoft Excel.
2. Click on the 'File' tab located in the upper left corner of the window.
3. At the bottom of the pop-up menu, clidk on Options.
3. Click on the 'Trust Center' tab.
4. Click on 'Trust Center Settings'.
5. Click on 'Macro Settings'
6. Place a check-mark in the 'Trust access to VBA project model' check box within the 'Developer Macro Settings' section.
7. Rerun the report.

** Ensure that Macros are enabled within MS Excel.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more