Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What type of RS485 cable is required for daisy-chaining Enercept meters?
Issue
What RS485 cable is required to wire Enercept meters.

Product Line
Enercept Meter

Environment
Communication Wiring

Cause
A twisted pair type of cable should be used in order to reduce radiated emissions and improve immunity of the communications system to any external electromagnetic interference.

Resolution
The Enercept meter has a 2-wire RS485 port. Belden 1120A, 9841 cable or equivalent cable is recommended to communicate or daisy chain with Enercept meters.

Schneider Electric Egypt and North East Africa