Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Internal Modbus register list for CM3000 and CM4000 Series Meters

Issue
Modbus list is needed

Product Line
CM3000 Series
CM4000 Series

Environment
Modbus Communications to CM3000 and CM4000 meters

Cause
Register list is needed to read registers when not using ION Setup or Power Monitoring Expert


Resolution
See the attached Register List.

Schneider Electric Egypt and North East Africa

Attachment(s)
Internal_CM3_CM4_Register_List_15_020.xls [4.88 MB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: