Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Analog Output Specifications for I/O External Expander Module Option D of the ION8600/ION8650 meter

Issue:

Recognizing  I/O of an external expander for ION8600/ION8650 meters.

Product Line:

ION8650- P850EB0

ION8600- P850EA0

Environment:

ION8650 Expander I/O Module

Cause

User couldn’t identify and wire the ION8650 meter Expander I/O module

Resolution:

Click the link for each model for more information: P850EA0/P850EB0 digital I/O expander module.

module.

  1. A-1 is 0 to 20 mA
  2. A-2 is 0 to 20 mA
  3. A-3 is -1 to 1 mA
  4. A-4 is -1 to 1 mA

Schneider Electric Egypt and North East Africa

Attachment(s)
Expander External user manual.pdf [865.59 KB]