How can we help you today?

Do ION meters log the IP address and user name used to modify Advanced Security passwords or settings?

Issue

Customer would like to know if ION devices log the IP address and username that is used to modify the Advanced Security passwords and/or settings.

Product Line

ION Devices

Environment

Hardware

Cause

Customer cannot find documentation on this specific characteristic of the ION device(s)

Resolution

ION meters with advanced security will log the source of the change (ethernet, serial), but do not provide any further information. This has been submitted as a future feature request.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center