Issue
There is no good way to reset Peak Demand on the PM800 series (among other Powerlogic Devices referenced)
Product Line
ION Enterprise
SPM7
Power Monitoring Expert (PME) 7.x
Power Monitoring Expert (PME) 8.x
Power Monitoring Expert (PME) 9.x
Power Monitoring Expert (PME) 2020
Power Monitoring Expert (PME) 2021
Power Monitoring Expert (PME) 2022
Power Monitoring Expert (PME) 2023
Power Monitoring Expert (PME) 2024
PM800
PM3000
BCPM
EM4000
Environment
PME Designer VIP
Resolution
The attached process will reset the Power Min/Max Demand at the start of every month, based on when the 'Clock' determines that a new month has began--not '30 days elapsed'.
This process can be used for other values that should be reset at the start of every month as well, so long as it is a value that the register is accessible via ION Enterprise.
Please check the attachments to download instruction file: 'Clock Based Reset Instructions'.
Released for: Schneider Electric Egypt and North East Africa