Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Modubs Register for Digital Input 1 (DI1) for a 7650

Not all modules have a hard-coded register to read; digital Input 1 (DI1) for the 7650 is and example of such.
If there is a need to read a module that does not have a hard-coded register, map that module to a modbus slave module and read the modbus slave modules output register.


Legacy KB System (APS) Data: RESL212298 V1.0, Originally authored by EdFa on 08/14/2013, Last Edited by EdFa on 08/14/2013
Related ranges: ION7550/ION7650