Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Which Modbus functions are used for reading/writing multiple data on IO scanning in Modicon Quantum range.
In Modicon Quantum range, I/O scanning works with following Modbus function codes:
  1. FC3 for Reading Multiple 4X registers.
  2. FC16 for Writing Multiple 4X registers.
  3. If both the read and write are filled out then FC23 for Read/Write Multiple 4X registers is used.