Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we use Prisma G and P with Direct Current (DC) ?
Prisma G & P can be used in DC current. Just pay attention to the following information:
The installations in DC current should be set up on the same way as AC current.The rated current indicated on the different Prisma Plus components (Multiclip, Polypact...) are the same for both installation types. The only characteristic to be taken into account is the devices Icc, root mean square current (RMS current) which should be higher than the installation DC Icc.

Concerning the design, as for AC installation, it is necessary to follow the instruction manuals and the configurations recommended in the catalogue.

For a DC current installation, you can use a linergy busbar, just taking 2 linergy bars in a 150mm duct, one for the minus (-) and one for the plus(+). The connections should be in accordance with the current of the
connected load.