How can we help you today?

Can the Circuit Monitor Series 2000 Alarm on Loss of Power?

If the load the CM2000 is monitoring loses voltage on any ONE phase, the CM2000 has the ability to alarm on this. The specific alarm is Voltage Loss (Alarm #31), which is an alarm that will become active when any ONE phase drops below the user-defined pickup value. The alarm will NOT become active if all three phases drop below the pickup value.
This specific alarm can be associated with the operation of a relay output on an ION, if installed.

Note: If the meter loses control power, there is no ability to signal the Voltage Loss alarm unless the CM2 Ride-Through Module is installed.

Note: The same applies for subsequent Circuit Monitor models and PM800 series meters. These meters have no ride-through module option.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center