Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the settings for a serial powered optical probe?

For serially connected optical probes (which do not have PS2 pigtail power) like the UNICOM III. The correct settings would be:
In ION setup> >Serial> Settings the RTS or DTS needs to be set to "Force ON".

Serial setup

Serial settings

Schneider Electric Egypt and North East Africa