Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between a Class 10 and Class 20 Power Meter?

Issue
What is the difference between a Class 10 and Class 20 Power Meter?

Product Line
Power Meters

Environment
ANSI C12.1 Standard Compliance

Resolution
The class system for power meters is defined by ANSI C12.1. The main difference between Class 10 and Class 20 meters relates to their maximum current rating and associated test currents.

ClassMax CurrentMeter TypeTest Current (F/L)Test Current (L/L)Test Current (50% PF)
1010 AInstrument-Rated2.5 A0.25 A2.5 A
2020 AInstrument-Rated2.5 A0.25 A2.5 A

  • Class 10 meters are designed for a maximum current of 10 A.
  • Class 20 meters are designed for a maximum current of 20 A.
  • Both classes share the same test currents for Full Load (F/L), Light Load (L/L), and 50% Power Factor conditions.

1

Last Revised: November 19, 2007
Public
All content © 1992-2007 Schneider Electric

Legacy KB System (APS) Data: RESL189300 V1.0, Originally authored by KBAdPM on 11/20/2007, Last Edited by KBAdPM on 11/20/2007
Related ranges: Standards Applied to Power Management PRODUCTS

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center