Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are there any known and recommended 10Base-FL fiber switch providers?


Issue:
ION Meters use 10Base-FL fiber connections. However, most suppliers only have 100Base-FL fiber switches.

Product Line:
ION8800, ION8600, ION7550/7650

Environment:
Fiber Connections

Cause:
Most suppliers only have 100Base-FL

Resolution:
The following suppliers are recommended 10Base-FL fiber switch providers:
Allied Telesyn
Website: http://www.alliedtelesis.com/

Transition Networks
Wedsite: http://www.transition.com/