Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Current Clamp wiring configuration with ION meters

Goals and Symptoms

Users may order the following current clamps to use with our ION meters:

Model #
Type
Current Range
Output
M1UB10A1V-10A
clamp-on
50mA to 10A AC
1 VAC
P32.UE.P813-1000A
clamp-on
1 to 1000A AC
1 VAC
P32.UE.P815-3000A
clamp-on
3 to 3000A AC
1 VAC
SCT0750-005-5A
split-core
5A
0.333 VAC
SCT1250-300-300A
split-core
300A
0.333 VAC

These clamp come with three wires
  1. Blue
  2. White
  3. Shield (If ordered separately from the meter).

Which wire is positive and which is negative?

Causes and Fixes

The Blue wire is the POSITIVE wire and should be connected to I11, I21 or I31
The White wire is the NEGATIVE wire and should be connected to I12,I22 or I32.
The Shield wire can be grounded.