Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PowerLogic High Density Metering (HDM) System 1-Meter & 4-Meter Enclosure Installation Guide, Instruction Bulletin

Issue
Require installation manual for high density meter enclosures.

Product Line
High density meter enclosures

Environment
Installation

Resolution

For the current HDM enclosure offer (including support for the PM5000 series meters), please see: FA272669


Manuals for older model HDM enclosures:
1 - Meter:    70000-0286-01
4 - Meters:    7002-0289-00

Schneider Electric Egypt and North East Africa

Attachment(s)
7002-0289-00.pdf [1.09 MB]
70000-0286-01.pdf [1.59 MB]