Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
The ION7500RTU meter does not accept the .dcf meter template file via ION Setup and returns the error message: "Unable to download dcf(xml) file to a non-RMP device"

Issue

When attempting to send a .dcf meter template file to the ION7500RTU using ION Setup, the process fails and displays the error:
"Unable to download dcf(xml) file to a non-RMP device."

Product

ION7500RTU Meter

Environment

  • ION Setup software
  • ION7500RTU device

Cause

Rapid Meter Programming (RMP) is not supported on ION7500RTU meters. The .dcf file format is designed for meters that support RMP, so it cannot be applied to this device.

Resolution

Use the .fwn version of the meter template file with ION Setup instead of the .dcf file. ION Setup will treat the .fwn file similarly to how it handles .dcf files on RMP-supported meters. Refer to the attached template file for the correct format.

Schneider Electric Egypt and North East Africa

Attachment(s)
7500-RTU_V1.1.0.fwn [311.72 KB]