Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Modem initialization string for the ION7650 and ION7550?

Issue
Modem initialization string for the ION7550/7650

Product Line
ION7550
ION7650

Environment
Communication Protocols

Resolution
The modem initialization string for the ION7650 and the ION7550 is 'AT&F' (without the quotes).