How can we help you today?

What are the Integer Register Multipliers for the Enercept Meter and Energy Meter?

Issue
A user needs the integer multipliers for the Energy Meter or Enercept Meter registers to correctly interpret the values.

Product Line
Energy Meter and Enercept Meter

Environment
Modbus Registers

Cause
An integer multiplier is required to properly scale and interpret the raw register values read from the device.

Resolution
The integer multiplier depends on the CT (Current Transformer) size used in the installation. The correct multiplier must be applied to the raw register values to obtain accurate measurements.

Please reference to the attached tables for the Energy Meter and Enercept Meter to determine the correct multiplier based on the CT size configured in the system.

Schneider Electric Egypt and North East Africa

Attachment(s)
Energy_Meter_Integer_Multiplier.pdf [13.84 KB]
Enercept_Meter_Integer_Multiplier.pdf [17.81 KB]