Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which phase does an ION8600 and ION8800 meter choose to measure frequency on?

Issue
Which phase does an ION8600 and ION8800 meter choose to measure frequency on?

Product Line
ION8600, ION8800

Environment
ION8600 and ION8800 meters in any voltage wiring configuration.

Resolution
An ION8600 and ION8800 series meter chooses the phase on which to measure frequency in a pseudo-random fashion, with a preference for Phase A more often than any other phase. The selection process is designed to account for unattached phases and will skip any phases that are not wired. This ensures accurate frequency measurement even in cases where only one or two phases are connected.


1
Date Created: November 27, 2009
Last Revised: December 23, 2009
Public
Original Author: TO
All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL200781 V1.0, Originally authored by MiNe on 12/23/2009, Last Edited by MiNe on 12/23/2009
Related ranges: ION8800, ION8600

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center