Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Dielectric Withstand Voltage of the ION6200 Communications Port?

Issue
What is the Dielectric Withstand Voltage of the ION6200 Communications Port?

Product Line
ION6200 Power Meter

Environment
ION6200 RS-485 Communications Port

Resolution
The maximum voltage that can be applied to the RS-485 communications port in the ION6200 is 7.5 Volts.