Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the VTFB-6 or CTSB-10 that is mentioned in the Terminal Block Assembly Wiring Technical Note still sold?
Issue:
A user has documentation that mentions fuse blocks and shorting blocks with part numbers VTFB-6 and CTSB-10. They are not able to find these part numbers as being valid in their ordering tools.

Product Line:
Shorting blocks and terminal blocks.

Environment:
Purchasing.

Cause:
VTFB-6 and CTSB-10 are not available anymore. The file that listed them initially was titled Terminal Block Assembly Wiring Technical Note with document number 70072-0129-07 (see attached file “Terminal Block Assembly Wiring 70072-0129-07.pdf”).

Resolution:
The shorting block part numbers are now 3090TB4 (4 pole) and 3090TB6 (6 pole) (see attached file “3090TB4 3090TB6 dimensions.pdf”).

Fuse block equivalents can be purchased from your local electrical distributor. Here is a link to find a distributor near you:
https://www.se.com/us/sites/us/en/support/distributor-locator/distributor-locator.page

Schneider Electric Egypt and North East Africa

Attachment(s)
3090TB4_3090TB6_dimensions.pdf [40.85 KB]
Terminal_Block_Assembly_Wiring_70072-0129-07.pdf [369.31 KB]