ProEssentials AcitveX: this ActiveX control is a graph library used to display Trending and Forecasting data on the meter webpage.
PUBLICATION NOTE: This document is published here under the FAQ document type because it is much easier and faster to make the document available on the appropriate powerlogic knowledgebase portals using the APS software tool than by using the strictly more appropriate (but generally more time-consuming) Schneider EDMS publication tool.
Legacy KB System (APS) Data: RESL205109 V1.0, Originally authored by ViWa on 04/16/2011, Last Edited by ViWa on 04/16/2011
Related ranges: ION7500/ION7600
Released for: Schneider Electric Egypt and North East Africa