Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I get the Serial Number, MAC address, firmware version for my EM4800?

Issue
How to determine the Serial number, MAC address or firmware version for the EM4800 meter.

Product
E4800 and EM4800

Environment
Web Browser

Resolution
1) Connect to the meter's web page using http://[IP address]
2) Click on the 'Info" menu option
3) Click on the "Manufacture" link

MAC address and serial number are also printed on product labels