Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum allowable main board temperature you can see in the diagnostic module of an ION8600?

Product Line
ION8600

Resolution
There is a main board temperature in the diagnostic module of ION meters; for the ION8600, the maximum allowable temperature is 85C. Anything above that will reduce the operation of the meter. The range of values which can be seen are from -55C to 125C. A value of 127 is displayed during a fault condition.