Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
E4800, EM4800, EM4000 Tenant Meter Guides / Manuals / Instructions

Article available in these languages: Spanish

Issue
Installation or Configuration guide is required for E4800/EM4800/EM4000 Series Meters.

Product Line
EM4800, EM4805, EM4833, EM4880
EM4000, EM4033, EM4080
E4805, E4833, E4880

Environment
Installation Guide, Configuration Guide, Manuals, Instruction bulletin

Cause
Unable to install and/or program the meter without the Configuration and Installation guide.

Resolution
There are 2 individual attachments for each of E4800, EM4800 and EM4000 Series meters for the Installation and Configuration Guide. See attached documents below.

Schneider Electric Egypt and North East Africa

Attachment(s)
EM4800_Configuration_Guide.pdf [833.68 KB]
EM4000_EM4800_Configuration_guide.pdf [1.54 MB]
EM4800_Installation_guide.pdf [2.74 MB]
EM4000_Installation_Guide.pdf [3.22 MB]
E4800_Installation_Guide.pdf [1.78 MB]
E4800_Configuration_Guide.pdf [1.93 MB]