Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you adjust the grid spacing in Vijeo Designer?

Issue:
Adjusting the grid spacing in Vijeo Designer


Product Line:
Vijeo Designer


Resolution:
In the Property Inspector field for Graphical Panels you can adjust the GridXSpacing and GridYSpacing.
image1

    • GridXSpacing defines the amount of spaces (shown in dots) for the horizontal grid.
      GridYSpacing defines the amount of spaces (shown in dots) for the vertical grid.
      When setting these properties, use a value between 1 and the Maximum. The Maximum is one-half of the height
      defined in the Panel Size for the target machine. For example, if you select SVGA 800 x 600 in the Panel Size field,
      the value of the Maximum is 300 (Y) and 400 (X).

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Center

    Find support resources for all your needs, in one place.