Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What do the "Tvs" parameters mean in the setup registers of the Harmonics Measurement Module?

Product Line

ION7550/ION7650

ION8800

PM8000

Environment

ION Framework

Resolution

'Tvs value' stands for 'Time versus Value'. These are 3 second rms values.

There is no upper limit for pulsing the evaluation input and there is no point in pulsing this module more frequently than 1x/second. By default is updates every 1 second.

If the Evaluation input is not linked and the Tvs Aggregate or Tvs Maximum mode is selected is select, a 3 second interval will be used.

Aggregate: the output of the module will be the 3 sec average harmonic (average of the 3 x 1 second Tvs values).

Maximum: then the output will be the largest value of the 3 x 1 second values.

Demand input is only used when display mode is set to Magnitude Outputs Displayed as Percentages or the THD Display Mode is set to Percentages. The input would a value like V1 Tot HD from a harmonics Measurement Module

Schneider Electric Egypt and North East Africa