Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the meaning of non tripping time in short time protection fixed time delay and instantaneous in micrologic 2 ?
Please note that if the current exceeds the pick up current, the non tripping time is the time of the micrologic unit that will not respond below it

i.e , if we have a fault current value which exceeds the pick up current  so the micrologic trip unit will not be able to respond in a duration less than the non tripping time.

but to be noted that in case of reflex tripping , the breaker mechanism will takes the protection action

Please check the attached PDF from the glossary of the NSX MCCB which explains this .

Schneider Electric Egypt and North East Africa

Attachment(s)
non tripping time in the glossary.pdf [1016.59 KB]