Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
We experience problems in developing the communication channel between MiCom Px20s (P123 & P220) and S1 through front port serial communication ?
Please focus first to the conncetion parameters settings and connection port of your PC.
If you use PC with Micom S1 Studio direct connected to the front panel port of the relay and do a quick connection to relay, you need to setup the connection parameters.
Password, do not change, keep it default.
COM Port is the com port of your PC. Default is COM 1.
If you use other (USB or other port) you need to specify which is.
Baud rate you can keep default 19200 or change to 9600.
Device address default is 1, but if you've changed by HMI specify the correct address.
Parity is Even by default but you need to check if PC COM port is setup with default Even parity.

Please focus on the connection between PC and relay and on the settings of your laptop rather than on relay itself.
If the connection is correct and the settings are correct, relay will answer.

Mind bellow notes:

PC: Command blocking 003 182
When command blocking is activated, commands are rejected from the PC interface.
PC: Sig./meas.val.block. 003 086
When signal and measured value blocking is activated, no signals or measured data are transmitted through the PC interface