Issue:
Does ATV61HC11N4T1 comes with a DC choke?
Product Line:
Altivar 61, Altivar 71
Environment:
ATV61/ATV71HD55M3X-HD90M3X, ATV611HD90N4-HC63N4, ATV71HD90N4-HC50N4. (including T1 and/or S383 suffix)
Cause:
Is the DC Choke included or does it need to be ordered separately and if so, what is the part number?
Resolution:
The part numbers listed above do require an external DC choke. This DC choke is included with the drive when ordered and does not need to be ordered separately. It does ship separately though.
Does ATV61HC11N4T1 comes with a DC choke?
Product Line:
Altivar 61, Altivar 71
Environment:
ATV61/ATV71HD55M3X-HD90M3X, ATV611HD90N4-HC63N4, ATV71HD90N4-HC50N4. (including T1 and/or S383 suffix)
Cause:
Is the DC Choke included or does it need to be ordered separately and if so, what is the part number?
Resolution:
The part numbers listed above do require an external DC choke. This DC choke is included with the drive when ordered and does not need to be ordered separately. It does ship separately though.
Released for: Schneider Electric Egypt and North East Africa