Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement of the Magelis XBTGT5230?

Issue:
Replacement for the Magelis XBTGT5230

Product Line:
XBTGT, HMIGTO


Resolution:
XBTGT5230 has been replaced with the HMIGTO5310

    • Vijeo Designer applications are 100 % compatible with automatic screens resizing.
      The cut-out is identical.
      The communication ports are identical except on COM1 , no RS422 signal only RS232C
      For RS422 link , use a cables with converter like TSXPCX1030 for Schneider Twido/Premium PLC or XBTZG919 + XBTZ980 for Mitsubishi FX PLC
      Same certifications.
      No extension Bus for Fieldbus modules ( Profibus , DeviceNet , CANopen )
      Only one USB port Host type A
      No auxiliary interface for speaker or alarm output
      Better Screen color TFT 65K and bigger Screen Size 121 , More Flash Memory , addition mini-USB Device port and use of SD card slot.

Schneider Electric Egypt and North East Africa