Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Negative Power Flow and Readings for kW, kVAR, and kWh

Product Line
CM4000 series
CM3000 series
CM2000 series
CM100/200 series
PM800

Environment
Measurements

Resolution
The only two readings that will change with negative powerflow are kW and kVAR. kWh will change only if the Circuit Monitor is in Signed mode. The default mode for the Circuit Monitors is Absolute mode.

Note: ION Meters only have Absolute mode.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center