How can we help you today?

ION 8650 Modbus and DNP values do not scale correctly

Issue
Scaling of DNP and Modbus output values may be incorrect when the PT ratio is set at 1:1. This will turn on the Scaled Operational Values output prematurely. It should only be enabled when BOTH the PT AND CT ratios are set to 1:1.
ION8650 Variant A

    • - 8650A_RMICAN_35S_V4.1.0.0.5.dcf
      - 8650A_RMICAN_V4.1.0.0.5.dcf
      - 8650A_V400_FAC-35S_V4.1.0.0.2.dcf
      - 8650A_V400_FAC_V4.1.0.0.2.dcf
      - Any framework derived from the above frameworks, including all prior revisions.
ION8650 Variant B
    • - 8650B_RMICAN_35S_V4.1.0.0.5.dcf
      - 8650B_RMICAN_V4.1.0.0.5.dcf
      - 8650B_V400_FAC-35S_V4.1.0.0.2.dcf
      - 8650B_V400_FAC_V4.1.0.0.2.dcf
      - Any framework derived from the above frameworks, including all prior revisions.
ION8650 Variant C
    • - Is not affected

Product

ION8650A

ION8650B

ION8650C

Enviorment

ION Meters

Cause
An incorrect formula is populated within the Arithmetic 74 (SetRatios1) formula 1 for the A and B variants (C variant is correct).
The incorrect formula on Variant A and B is IF(S1=S2,1,0), which can be seen below.

formula

Resolution
The corrected formula can be seen below as IF(AND(S1=S2,S3=S4),1,0)
formula corrected

The fix to this formula can be done directly in unlocked meters using IONSetup or Designer, or download the corrected template listed below.

These formulas have been fixed in:

ION8650 Variant A

    • - 8650A_RMICAN_35S_V4.1.0.0.6.dcf
      - 8650A_RMICAN_V4.1.0.0.6.dcf
      - 8650A_V400_FAC-35S_V4.1.0.0.3.dcf
      - 8650A_V400_FAC_V4.1.0.0.3.dcf
      - Any framework derived from the above frameworks.
ION8650 Variant B
    • - 8650B_RMICAN_35S_V4.1.0.0.6.dcf
      - 8650B_RMICAN_V4.1.0.0.6.dcf
      - 8650B_V400_FAC-35S_V4.1.0.0.3.dcf
      - 8650B_V400_FAC_V4.1.0.0.3.dcf
      - Any framework derived from the above frameworks.
ION8650 Variant C
    • - Is not affected

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center