How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

Which HMI ranges can be connected directly can beto zelio logic smart relay ?

Magelis STO 501 terminal is dedicated exclusively to communication with ZelioLogic SR2/SR3 range controllers.

It communicates with these controllers via a direct connection cable SR2 CBL 09, using Zelio protocol, which is included in Vijeo Designer V6.1.

Also XBT N401, XBT R411 and XBT RT 511 can have direct connected with Zelio with  SR2 CBL 08 cable, using Zelio protocol, which is included in Vijeo Designer Lite V1.3.

Schneider Electric Egypt and North East Africa
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
  • Help and Contact Center