Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the difference between LC1D**** and LC2D**** references from the Tesys "D" range ?
The LC1D**** is normal contactor used to control switching on and off of uni-directional motor

The LC2D*** is a two contactors from LC1D mechanically interlocked together used to control the bi-directional motor or used in reverse motor applications

Note that we can perform the LC2D**** using two LC1D*** with separate mechanical interlock