Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the message - Circuit Trip - mean on a Sepam Relay Series 20/40/80?

Goals and Symptoms

What does the message - Circuit Trip - mean on a Sepam Relay Series 20/40/80?

Causes and Fixes

The Circuit Trip is related to the CB control features. It indicates that the Input I11 or input I12 on Sepam is not receiving a signal. If you are not using a Circuit Breaker control the recommendation is not to use this function.

**************************

Original article#3619

Re-published to revised security level: 17 June 2008 by DRM

Public

All content © 1992-2007 Schneider Electric

**************************

Legacy KB System (APS) Data: RESL185670 V2.0, Originally authored by KBAdPM on 06/29/2007, Last Edited by DaMi on 06/18/2008
Related ranges: Sepam series 80, Sepam series 40, Sepam series 20

AEDL3

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center