Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to use MBMaster to verify basic modbus communications.

Issue
Using MBMaster to verify that a Modbus device is working.

Product Line
Modbus devices

Environment
Windows

Cause
MbMaster can be used to determine if a modbus device is working.

Resolution
Run this program from a DOS prompt.

For example here is a sample where I connect to a 6200 device at 19,200 baud. I am using the PC's COM2. The meter's Unit ID is 100 and it is configured to use the Modbus protocol. I am asking for Modbus address 44000 which provides the password for this meter. My meter's password is 0.

MBMaster provides quite a bit of diagnostic information which you can ignore in this case. Just look for the data from the register.

-=-=-=-=-=- Sample MBMaster -=-=-=-=-=-=-=-
H:\\Bin>mbmasterV21M3 -COM2 -B19200 -ID100 -SR44000 -NR1
MBMASTER v2.1M3:    Compiled at Jul 13 2001 04:13:57

Stripped BAUD from input: 19200
Stripped SR from input: 44000
Install ModPL
About to open ModPL with port COM2
Building request: modslave = 100
Modbus AL frame received: fc = 03
Modbus AL frame: startreg = 404000, #regs = 1
Register 404000: 0
Exiting.
-=-=-=-=-=- End Sample MBMaster -=-=-=-=-=-=-=-

  • Original article#9458

    Controlled

    All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189023 V1.0, Originally authored by KBAdPM on 11/09/2007, Last Edited by KBAdPM on 11/09/2007
Related ranges: Modbus / JBus

Schneider Electric Egypt and North East Africa

Attachment(s)
MBMaster.zip [47.14 KB]