Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to configure the Momentum to start in RUN mode after a power cycle using Modsoft

Issue
How to configure  a Momentum start  in 'RUN' mode after a power cycle using Modsoft.

Product Line
All Momentum PLC's.

Environment
Windows 7

Resolution
In order for the Momentum to start in RUN mode after power cycle, the program must be saved to the built-in flash.
The following steps can be used to accomplish this in 'Modsoft version 2.62.

  • Click Online\ Direct To PLC.
  • Press F2 'PlcOps'.
  • Press F2 to 'Stop the PLC'.
  • Press F8 'Save To'.
  • Type in Y for answering the question (Continue Power Down Run State?).
  • Type in Y for 'Continue'.
  • Press F1 to 'Start the PLC'.
  • Disconnect from the PLC.
  • Power cycle the PLC and it will start back up in RUN mode.

Schneider Electric Egypt and North East Africa