Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
TSXETC101 Explicit Messaging CIP Modbus Object Read Example

Issue
The attached document is a CIP Modbus Object Read example for a TSXETC101 using the Send_Req block to read from a Quantum 140NOC77101.



Product Line
Premium TSXETC101

Quantum 140NOC77101
M340 BMXNOC0401


Resolution
This example will read from located registers in Schneider PLC's with the following network modules installed:

  • TSXETC101
  • 140NOC77101
  • BMXNOC0401

This example does not apply to reading from located registers in Schneider PLC's through the following network module:
  • 140NOC78000



(Removed File URL: 210428_45B6/TSXETC101_CIP_Modbus_Object_READ_Example.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/b0d88c9927345b0dc1257afe002cc849/fl_block_5/0.120?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL210428 V1.0, Originally authored by DaDz on 01/25/2013, Last Edited by DaDz on 01/25/2013
Related ranges: Modicon Premium

Schneider Electric Egypt and North East Africa

Attachment(s)
TSXETC101_CIP_Modbus_Object_READ_Example.pdf [128.14 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center