Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to find the Firmware Version or Serial Number of any ION or ACM device using ION Setup

Product Line
ION Meters
ION Setup

Environment
ION Setup Diagnostic

Resolution
The Firmware version and Serial Number of any meter (Legacy ACM or ION) can be found in ION Setup by following the steps below.

  1. Open ION Setup.
  2. Add the device to ION Setup. See the ION Setup User Guide in FA346479 for instructions.
  3. Click the device of interest
  4. Select Meter Diagnostics 1 in the ION Setup toolbar.
  5. Select the General tab to view the Firmware version and Serial Number of the meter.

2

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center